The cycle-accurate simulator for RH850 is the instruction simulator to allow you to measure execution times with accuracy close to times on the actual machine through the use of a PC environment alone.
Verify operation by using the simulator set up for cycle accuracy interlinked with the Embedded Target for RH850 Multicore. You can also use the simulator in advance evaluation of the performance of an RH850 device even in an environment with neither the actual machine nor an emulator.
A setting file and a license key are provided as follows for each supported series (the simulator does not cover all devices in the series).
The CS+ simulator performs as a cycle-accurate simulator when the license key is registered with the license manager after installing the information file for cycle accuracy on the PC on which the CS+ integrated development environment has been installed.
Unless the above situation is set up, the simulator continues to perform as an instruction simulator which is not cycle-accurate.
Contact your local Renesas Electronics marketing office or distributor if you wish to introduce or obtain detailed information on these tools.
Series | Applicable MCU (Note1) | Status |
---|---|---|
RH850/C1x | RH850/C1H, RH850/C1M-A1, RH850/C1M-A2 | Yes |
RH850/E1x | RH850/E1M-S2 (Note2) | Please contact us. |
RH850/E2x | RH850/E2M, RH850/E2UH, RH850/E2H | Yes |
RH850/F1x | RH850/F1K, RH850/F1KH-D8, RH850/F1KM-S4 | Yes |
RH850/P1x | RH850/P1H-C, RH850/P1M, RH850/P1M-C, RH850/P1M-E | Yes |
RH850/U2x | RH850/U2B6, RH850/U2B10 | Yes |