TO-5-Packaged Single- and Dual-Channel Detectors Provide Industry’s-Best Performance, Quality, and Longevity for CO2 Sensors
TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today expanded its industry-leading environmental sensor portfolio with its first family of thermopile-based detectors with integrated optical filters for optical (NDIR) CO2 sensors. The four new single- and dual-channel analog detectors for CO2 gases deliver the industry’s best performance, quality, and longevity in a TO-5 package, making them ideal for use in a variety of industrial, medical and IoT applications that require high reliability, high accuracy and operation in high temperatures.
CO2 levels are a major component of indoor air quality (IAQ) measurement, and thermopile-based detectors are a key building block of sensing solutions required by applications such as HVAC control, air quality monitoring, surgical equipment, and capnography equipment for ventilator systems. Renesas’ new detectors deliver fast response times with a time constant ranging from 18 to 25 ms and a high signal-to-noise ratio ranging from 1,981 to 4,953 to ensure the accuracy required for mission-critical applications where high reliability is a must. The devices are certified for high temperature environments, supporting applications operating with extended temperature ranges up to 125°C.
The new thermopile-based detectors complement Renesas’ current environmental sensor lineup for air quality detection. Customers can combine CO2 sensors based on the new detectors with a variety of Renesas sensors such as its popular ZMOD4410 IAQ platform featuring embedded AI and an IP67-rating package option, and/or its HS3001 high-performance, highly accurate relative humidity and temperature sensor. Together with Renesas microcontrollers (MCUs), this combination enables customers to create a complete environmental sensing solution for medical or industrial applications.
“With more people spending longer hours indoors during current events, many home, healthcare, educational, and work environments are adopting HVAC systems and equipment with increasingly sensitive detection features to ensure healthy CO2 levels,” said Uwe Guenther, Senior Director, Sensing Solutions, IoT and Infrastructure Business Unit at Renesas. “Renesas’ new family of thermopile-based detectors support the development of the highest performance CO2 sensors, enabling manufacturers of HVAC systems and other medical and industrial applications to meet the changing requirements for CO2 detection at an affordable price point, delivering real-time feedback for these mission-critical applications while maintaining high accuracy and reliability.”
Renesas has also combined the new thermopile-based detectors with its complementary analog and power devices and Dialog’s Bluetooth® Low Energy system on chip to create the new Thermopile CO2 Detector Winning Combination, which can be used to detect ambient CO2 concentrations. Renesas offers more than 250 Winning Combinations with compatible devices that work together seamlessly for a wide range of applications and end products. They can be found at renesas.com/win.
Availability
The RH5Z0610D, RH5Z0622D, RH5Z1210D, and RH5Z1222D thermopile detectors and thermopile detector evaluation kit are available now from Renesas’ worldwide distributors. For more information, please visit renesas.com/thermopiledetectors.
About Renesas Electronics Corporation
Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, YouTube and Instagram.
(Remarks) Bluetooth is a registered trademark of Bluetooth SIG, Inc. All registered trademarks or trademarks are the property of their respective owners.
The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.