GR-PEACH is the Gadget Renesas board for the Renesas RZ family's RZ/A1H group of microprocessors (MPU) products. Fully pin-compatible with Arduino UNO, GR-PEACH is an Arm® MbedTM enabled development platform. GR-PEACH takes advantage of web browser-based program development and a robust library selection. With the added appeal of 10MB of built-in RAM and the processing power of Arm CortexTM-A, GR-PEACH was created for the developer interested in high-speed prototyping of IoT devices with loads of HMI—graphics, touch panel, camera input, audio, network and more.
In addition, RZ/A1H FreeRTOSTM Software Package for GR-PEACH has been released.
In addition, GR-PEACH supports multiple platforms, .NET Micro Framework (MF), Arduino, and TOPPERS/ASP (RTOS). Click the platform figures below to be directed to the respective getting started pages.
Embeds Arm Cortex-A RZ/A1H (R7S721001VCBG) and Arduino UNO pin compatibility supports various shields.
Corestaff vendor's site
GR-PEACH board is equipped with a LAN connector (RJ-45) and connectors for Arduino UNO compatible pins and service pins.
Corestaff vendor's site
Enables camera and Wi-Fi connection with the GR-PEACH board. Camera specifications are VGA 640 x 480, maximum 60fps and a horizontal angle view of 98 degrees.
Corestaff vendor's site
Enables stereo plug, camera module and USB host connection with GR-PEACH.
Note: A camera module is not included. MT9V111 is recommended.
4.3-inch wide display with touch panel.
Note: GR-PEACH-FULL cannot be used for this shield. Refer to the vendor's site for the use detail.
Corestaff vendor's site
CE, EU RoHS, China RoHS
The pin map below is for sketching with Arduino style on the Renesas web compiler. If the Mbed development environment is being used, visit the Mbed site.
Project file for sketching in Eclipse-based development environment e2 studio. For downloading and installing e2 studio, please refer to the e2 studio product page.
You can import as an archive file (zip) as an existing workspace from the e2 studio menu "File" -> "Import".
Do the menu "Project" -> "Update all dependencies" at the initial build. Only sources changed since the next build will be compiled.
DisplayApp is an application that displays the camera image sent by USB CDC.
Installing the USB driver is required on versions earlier than Windows 10.
Below is an Arduino-like sketch example.
#include <Arduino.h> #include <Camera.h> #include "DisplayApp.h" Camera camera; static DisplayApp display_app; void setup() { camera.begin(); } void loop() { display_app.SendJpeg(camera.getJpegAdr(), (int)camera.createJpeg()); delay(10); } }
Gadget Renesas provides boards that make it possible to prototype ideas quickly, a community where users can interact, and events to help users build their projects to make their ideas a reality. Below are some projects that utilized the GR-PEACH board.